What video recorder (if any) can I run full 8, 16 or 32 IP-based cameras?

Issue

What video recorder (if any) can I run full 8, 16 or 32 IP-based cameras?

Product Line

Pelco Cameras, Pelco Video Management

Environment

  • DSSRV- All versions
  • Endura Xpress- All versions
  • Endura system- All versions

Cause

Information regarding the available systems to record 8, 16 , or 32 IP based cameras is needed.

Resolution

You can choose from DSSRV to EnduraXpress to full Endura system. All three video management system will support 32 IP-based cameras.

DSSRV
The NVR comes preloaded with DS NVs Network Video Management Software and delivers 280 Mbps bandwidth for recording and viewing as many as 128 Pelco and third-party IP cameras. Analog cameras on the network are supported using encoders from Pelco or from a number of third-vendors.
*Click on the heading for DSSRV home page.

EnduraXpress
EnduraXpress combines the performance, reliability, and robustness of an enterprise-class, mission-critical storage management system into a compact, stand-alone unit. Aggressively priced, the EE500 effectively lowers the cost threshold for enterprise-class IP video performance, bringing affordable reliability to the 32- to 64-camera segment.
*Click on the heading for EnduraXpress home page.

Endura System
Delivers industry leading performance and innovation for mission-critical storage needs. The combination of high performance, scalable hardware design and advanced software capabilities enables the NSM5200 to meet the unique storage needs of physical security and video surveillance applications.
*Click on the heading for Endura home page.