Change the date and time on the CM9700 Matrix Switcher using the CM9760-KBD-US keyboard

Issue

How do I change the date and time on the CM9700 System?

Product Line

Pelco Matrix

Environment

CM9700 matrix

Cause

Current time in the CM9700 system is incorrect.

Resolution

You can manage or change the time on your CM9700 system directly from your CM9760-KBD keyboard.
Follow the steps below:

  1. Select the "DEF" icon on your display of your KBD. If  "DEF" is not available, select " ESC " or select "MORE".
  2. If prompted for a pin number, the default 1234. There should be an icon resembling a clock.
  3. Select the clock.
  4. Select option to input the DATE.
  5. Select the clock again to see the option to input the TIME.
  6. Input the time in 24-hour format.
  7. Select the clock icon once again to complete.