Maximum number of camera inputs for the CM6700/CM6800 Matrix Series

Issue

What is the maximum number of camera inputs for the CM6700/CM6800 Matrix Series?

Product Line

Pelco Matrix

Environment

  • CM6700 Series
  • CM6800 Series

Cause

Amount of cameras that can be physically connected to matrix by coaxial cable.

Resolution

Matrix Model Camera Inputs Monitor Outputs Data Ports
CM6700-MXB2 16 2 2
CM6700-MXB4 16 4 2
CM6800-32X6 32 6 6
CM6800E-48X8 40 loop 8 non loop total 48 8 10
CM6800-96X16 80 loop 16 non loop total 96 16 12