What is a Matrix Switcher/Controller?

Issue

What is a Matrix Switcher/Controller?

Product Line

Pelco Matrix

Environment

Matrix system

Cause

Function of a Matrix system.

Resolution

The 9780 System is a full-featured video matrix switching control system that allows users to view and control up to 4,096 cameras and 512 monitors on a single node. Expanded monitor capacity in the matrix bay allows implementation of larger systems with a smaller footprint (less hardware) than other matrix systems

The 9770 System is a full-featured video matrix switching control system that allows users to view and control up to 2,048 cameras and 512 monitors on a single node. Expanded monitor capacity in the matrix bay allows implementation of larger systems with a smaller footprint (less hardware) than other matrix systems.

The following link gives a break down of the different matrix switches available: Matrix Systems