What is the maximum number of controller (user) for the CM9700 Series Matrix Switcher System?

Issue

What is the maximum number of controller (user) for the CM9700 Series Matrix Switcher System?

Product Line

Pelco Matrix

Environment

CM9700 Series Matrix all versions

Cause

The differences between Matrix models is required.

Resolution

The CM9765 System is a full-featured video matrix switching control system that allows users to view and control up to 2,048 cameras and 512 monitors on a single node. Up to 96 individual user-defined ID numbers can be assigned to allow or deny access to system functions.

The CM9770 System is a full-featured video matrix switching control system that allows users to view and control up to 2,048 cameras and 512 monitors on a single node. Expanded monitor capacity in the matrix bay allows implementation of larger systems with a smaller footprint (less hardware) than other matrix systems. Up to 96 individual user-defined ID numbers can be assigned to allow or deny access to system functions.

The CM9780 System is a full-featured video matrix switching control system that allows users to view and control up to 4,096 cameras and 512 monitors on a single node. Expanded monitor capacity in the matrix bay allows implementation of larger systems with a smaller footprint (less hardware) than other matrix systems. Up to 96 individual user-defined ID numbers can be assigned to allow or deny access to system functions.

For more information, visit the Matrix Systems product page on pelco.com.