What is the CM9760-DMR Data Manager?

Issue

What is the CM9760-DMR Data Manager?

Product Line

Pelco Matrix

Environment

CM9760-DMR Data Manager

Cause

Product Specification.

Resolution

The CM9760-DMR is a data manager package that provides a four-to-one expansion of the number of data (SERCOM) ports available on a CM9760, CM9770, or CM9780 central processing unit (CPU). It may be used with System 9700 Series matrix switchers in three basic applications: To expand the number of cameras controlled through a port (Camera Control Expander), to expand the number of keyboards connected to a port (Keyboard Expander), and to interface up to four PTZ controllers to control a common group of cameras (Data Merger).