What ports on the CM6800E-48X8 support ASCII communication?

Issue

What ports on the CM6800E-48X8 support ASCII communication?

Product Line

Pelco Matrix

Environment

  • CM6800 Matrix Series

Cause

ASCII communication connection port of matrix

Resolution

There are 5 ports on the CM6800E-48X8 that support ASCII communication. The are a few differences when wiring.
 

Port# Wiring Default Device Programmable to Others Device
1 RS232 MANAGER ASCII
2 RS232 CM6800E-48X8 ASCII
4 RS485 GENEX ASCII
7 RS485 or RS232 ASCII  
8 RS485 or RS232 ASCII  

Click here for the ASCII list.

View the following related Lessons Learned articles: