How to create a camera name in the DX4500/DX4600 Series

NOTICE

DISCONTINUED PELCO PRODUCT.
This product has been discontinued. For further information please visit pelco.com/support/discontinued-products

Issue

How to create a camera name in the DX4500/DX4600 Series

Product Line

Pelco Video Management

Environment

  • DX4500
  • DX4600

Cause

Editing the camera name to match to scene location.

Resolution

To create a camera name, do the following:

1. On the front panel or remote control, press ENTER. Using the mouse, click CH 01. The channel 01 name box is highlighted.

2. On the front panel or remote control, press the up/down arrow buttons to highlight a channel, and then press ENTER. Using

the mouse, click a channel name box. The “Please enter the channel name” virtual keyboard opens.

3. To delete the existing name, on the front panel or remote control, press any of the arrow buttons to highlight the

backspace key , and then press ENTER. Using the mouse, click the backspace key until the name is deleted.

4. To type a name using the front panel or remote control, press any of the arrow buttons to highlight a character from

the virtual keyboard, and then press ENTER. Using the mouse, click a character. The selected character is displayed in the channel

name box.

5. Repeat step 4 until the camera name is typed in the channel name box.

6. To confirm the entry using the front panel or remote control, press any of the arrow buttons to highlight OK. Using

the mouse, click OK. The camera name is displayed in name box.

7. Repeat steps 2 and 3 to name other cameras.