B-tree and rebuild can not fix a problem in an access control file

Issue

B-tree and rebuild can not fix a problem in an access control file

Product Line

TAC I/NET

Environment

I/NET Access Control

Cause

You must first use the AC file conversion utility to convert it to a MDB format.

Resolution

  1. Select mdb as the target file type
  2. Open the file in Microsoft Access
  3. Delete the problem records
  4. Run the AC file conversion to reconvert it back to AC file type
  5. Run the conversion from 1.XX to 2.XX.