How do I adjust video level on the IS Camclosure Series?

Issue

How do I adjust video level on the IS Camclosure Series?

Product Line

Pelco Cameras

Environment

  • IS110-DN model
  • IS110-CH model
  • IS90-CHV9

Cause

Iris adjustment to open/close iris

Resolution

To adjust iris video level, follow these steps: 

1.Tilt or rotate the camera module until you can access the auto iris level control (R19).
2. Turn the screw clockwise to increase the brightness level or counter clockwise to decrease the brightness level.

The electronics of the IS Camclosures Series automatically adjust the camera to the auto iris. Therefore, auto iris level adjustments are not necessary.

 

Related lessons learned articles: