Is the Spectra IV IP compatible with the DX4000 Series digital video recorder (DVR)?

NOTICE

DISCONTINUED PELCO PRODUCT.
This product has been discontinued. For further information please visit pelco.com/support/discontinued-products

Issue

Is the Spectra IV IP compatible with the DX4000 Series digital video recorder (DVR)?

Product Line

Pelco Cameras, Pelco Video Management

Environment

  • DX4000
  • Spectra IV IP

Cause

Analog Video Connection

Resolution

The DX4000 supports the Analog video output signal option from the Spectra IV IP. Connect a coaxial cable from the DVR to the analog output on the Spectra IV IP.

Note: The DX4000 DVR does not have the capability to request for IP video stream, and therefore, will not be able to record video over network.