How do I validate PTZ permission credential on the Spectra IV IP?

Issue

How do I validate PTZ permission credential on the Spectra IV IP?

Product Line

Pelco Cameras

Environment

  • Spectra IV IP Series

Cause

Roles and Permissions

Resolution

To check permission credential, perform the following steps:

  1. Click Settings in the main menu; the Spectra IV IP settings menu opens
  2. Click the Roles tab; all defined roles are located in the box on the left side of the screen.
  3. Click on Defined Role; view the permissions enabled for the role.
  4. Enable Allow PTZ Control permission.
  5. Click Update button to save the new settings. Only users with PTZ control permission will be able to pant, tilt, and zoom.