Can the Spectra IV IP be powered via Power over Ethernet (PoE)?

Issue

Can the Spectra IV IP be powered via Power over Ethernet (PoE)?

Product Line

Pelco Cameras

Environment

  • SD4N Spectra IV series
  • SD4E Spectra IV Series

Cause

Power input to Spectra IV IP

Resolution

No. Spectra IV IP is not designed for PoE input option. Spectra IV IP is an analog camera converted to IP via encoder card only. The input power requirements do not change. Power requirement is 24VAC or 24VDC.

See Lessons Learned Article #10270 for Spectra IV outdoor requirements.