What is the difference between the Endura NET5400T Series Encoder and NET5301T or SP04-140?

Issue

What is the difference between the Endura NET5400T Series Encoder and NET5301T or SP04-140?

Product Line

Pelco Video Management, Pelco Transmission & Power

Environment

  • Endura NET5400T encoders- All versions
  • Endura NET5301T- All versions
  • Endura SP04-140- All versions

Cause

Information regarding the different encoders was needed.

Resolution

  • The NET5400T is a 1,2 or 4 channel H.264 video encoder.
  • The NET5301T is a single channel MPEG-4, standard definition video encoder.
  • The SP04-140 is a two-channel MPEG-4, standard definition video encoder.
Visit the Video Encoders page on pelco.com for complete details.