How do I perform a system recovery on the Endura WS5050, WS5060, and WS5070 workstations?

Issue

How do I perform a system recovery on the Endura WS5050, WS5060, and WS5070 workstations?

Product Line

Pelco Video Management

Environment

Endura WS5050, WS5060, WS5070 workstations

Cause

Workstation show blank screen after recovery.

Resolution

Select the corresponding guide below for system recovery instruction.

Endura WS5050 Software Recovery


Endura WS5060 Software Recovery


Endura WS5070 Software Recovery

WS5070 Recovery image downloads:

Windows Vista

Windows 7

note: Due to size, a dual-layer DVD must be utilized with the above file.