Adjust zoom speed on the Spectra IV SL and Spectra IV SE models

Issue

Where can I adjust zoom speed on the Spectra IV SL and Spectra IV SE models?

Product Line

Pelco Cameras

Environment

  • Spectra IV SL
  • Spectra IV SE

Cause

Adjust the zoom speed to increase/decrease the focus in when zoom button is pressed.

Resolution

Spectra IV SL:
There is no zoom speed setting in Spectra IV SL models.

Spectra IV SE:
To adjust zoom speed settings in Spectra IV SE models, follow the below steps:

  1. Go into the camera menu using the "preset 95" command.
  2. Using the "open iris" function, go into the "dome settings" section.
  3. Open the "camera" section using the "open iris" function.
  4. Select speed options: 
    Low 6.6 seconds
    Medium 4.6 seconds
    High 3.2 seconds
  5. Exit camera menu.