Experience intermittent control issues with Spectra IV version 1.08 or newer.

Issue

What to check when experience intermittent control issues with Spectra IV version 1.08 or newer?

Product Line

Pelco Cameras

Environment

Spectra IV version 1.08

Cause

Dip switch settings on the dome drive.

Resolution

If there are problems with control or behavior such as stopping when a pattern or preset has been called, verify that the DIP Switch 2-3 is set to the "ON" position. Setting the DIP Switch 2-3 to "ON" enhances Coaxitron communication, addresses problems with P and D protocol and may work with other 3rd party applications such as Dedicated Micros and other manufacturer's equipment.

Note: This only apply to Spectra IV version 1.08 and newer.