Troubleshooting a lighting controller circuit point that does not fire the relay

Issue

When controlling a circuit point in the summary, the relay does not fire.

Product Line

TAC I/NET

Environment

7780 Lighting Controller

Cause

 PICO Fuse on the 7780 controller may be burned out.

Resolution

Check the PICO Fuse on the 7780 controller. It may be burned out and need to be replaced. Also double check the Control Description.