Is the DX Series Client the same as the DX8100 PC Client?

Issue

Is the DX Series Client the same as the DX8100 PC Client?

Product Line

Pelco Video Management

Environment

  • DX Series Client
  • DX8100 PC Client
  • DX8100 Series recorders

Cause

Understand the differences between the two remote client software to meet the purpose of the site installation.

Resolution

No. However, the DX Series Client is compatible with the DX8100 Series DVR and can be used in place of the DX8100 PC Client. The DX Series Client is compatible with the product ranges DX4104, DX8100, DX4500/DX4600, DX4700/DX4800, whereas the DX8100 PC Client only support DX8100.