What version of Spectra IV firmware uses switch SW1-8 for coaxitron control and which one uses SW2-3?

Issue

What version of Spectra IV firmware uses switch SW1-8 for coaxitron control and which one uses SW2-3?

Product Line

Pelco Cameras

Environment

Spectra IV / IVse version 1.062
Spectra IV / IVse version 1.07

Cause

Firmware upgrade changes the enhanced coaxitron control dip switch setting.

Resolution

Spectra IV version 1.062 used SW1-8 for enhanced coaxitron control. Note that with the introduction of 1.07 firmware, the switch setting for enhanced coaxitron control was moved from SW1-8 to SW2-3.