Find the version number on the Spectra IV IP or Sarix camera

Issue

How do users find the version number on the Spectra IV IP camera?

Product Line

Pelco Cameras

Environment

  • Spectra IV IP
  • Sarix Series

Cause

Location of version number for Sarix or Spectra IV IP encoder card.

Resolution

To locate the firmware version, follow these steps:

  1. Enter the camera's IP address into a web browser.
  2. At the login prompt, log into web configuration menu using the following default credential:
    username: admin
    password: admin
  3. Once logged in, click Settings link on the top right of the screen.
  4. Under General tab, near the top, is the firmware version number.