How do users determine a Sarix camera's model and serial number?

Issue

How do users determine a Sarix camera's model and serial number?

Product Line

Pelco Cameras

Environment

  •  All Sarix Series

Cause

Model and Version of Sarix confirmation

Resolution

  1. Open the Web browser.
  2. Type the camera’s IP address in the browser address bar.
    NOTE: If you do not know the camera’s IP address, you can locate it using the Pelco Device Utility software. 
  3. Click the Login button in the navigation bar; a dialog box appears.
  4. Type your user ID and password.
    NOTE: If you are logging on to the camera as the administrator for the first time, the default User ID and Password are admin (all lowercase). For security purposes, be sure to change the password after you log on for the first time.
  5. Click Log In
  6. Next, click on the Settings link on the top left.
  7. The System tab's contents should be viewable. If not, click on the System tab. The serial number and model number are located on the bottom left of the screen.