How do I change a Spectra IV IP back to analog?

Issue

How do I change a Spectra IV IP back to analog?

Product Line

Pelco Cameras

Environment

  • TXB-IP-P
  • TXB-IP-F

Cause

Use of Analog and IP video.

Resolution

The Spectra IV IP has both analog and Ethernet outputs. There is nothing required to change to utilize analog signal. There is a pigtail located on the door assembly with a BNC connector attached that will output signal when the IP translator board is installed.

Related articles:

Why does the Spectra IV have no analog ptz control with the TXB-IP inserted?