Use Camera Security feature in the DX8100 Series Hybrid Video Recorder to covert camera.

Issue

How to use the DX8100 Series Hybrid Video Recorder "Camera Security" feature to "Covert" a camera.

Product Line

Pelco Video Management

Environment

DX8100 HVR Series

Cause

Enable security on the camera.

Resolution

  1. On the DX8100 toolbar, click the Setup button. The Setup dialog opens to the Camera page.
  2. In the Camera Properties section, do the following:
    1. Select a camera from the Channel drop-down box. Alternately, you can click a camera in the Site Tree to select it.
    2. Verify that Local Camera is displayed in the associated Selected Channel drop-down box.
    3. Set camera security level. The default security levels are as follows:
    • None: The camera can be viewed by all users.
    • Low: The camera can be viewed by all users except the Guest account.
      • NOTE: If you do not want video from a low security level camera to be viewed by the Guest user, set the security level for that camera to medium or higher.
    • Medium: The camera can be viewed by users with Standard User access and higher.
    • High: The camera can be viewed by users with Power User access and higher.
  3. Click Apply.