What is the maximum number of IP cameras supported by a single Digital Sentry NVR system?

Issue

What is the maximum number of IP cameras supported by a single Digital Sentry NVR system?

Product Line

Pelco Video Management

Environment

  • DSSRV
  • DS NVs
  • Digital Sentry NVR
  • IP cameras

Cause

Information about the total number of supported IP camera on the Digital Sentry NVR system.

Resolution

The maximum number of IP cameras a single Digital Sentry NVR (DSSRV) system support is 128 cameras. The software has a max limit of 280Mbps for incoming and outgoing network traffic.