Can the Sarix megapixel camera systems be focused using the DS ControlPoint client user interface?

Issue

Can the Sarix megapixel camera systems be focused using the DS ControlPoint client user interface?

Product Line

Pelco Cameras, Pelco Video Management

Environment

  • Sarix cameras with Auto Focus
  • DS Control Point

Cause

Sarix camera out of focus and needs to be adjusted

Resolution

No. Focusing the camera must be accomplished using the Sarix Camera Web User Interface, or through the Endura Utilities Application (see LL#14121) .