What is the default network IP address of the Endura NET5400T series video encoder?

Issue

What is the default network IP address of the Endura NET5400T series video encoder?

Product Line

Pelco Cameras, Pelco Video Management, Pelco Transmission & Power

Environment

Endura NET5400T encoder

Cause

Logging on to the encoder to access the encoder and its cameras

Resolution

Without a DHCP server, the default network settings are:
    IP address = 192.168.0.20
    Subnet Mask = 255.255.255.0


It is important to note that each video input on the 2 and 4-channel models is independent of each other. The first channel to come up will be assigned an address of 192.168.0.20, the next channel to come up will be assigned 192.168.0.21, and so on.