Multi-screen view on the CM6700/6800 Series Matrix.

Issue

How do I configure the CM6700/6800 Series Matrix to display in multi-screen view?

Product Line

Pelco Matrix

Environment

CM6700 Series Matrix
CM6800 Series Matrix

Cause

View multiple cameras on one screen.

Resolution

The CM6700/CM6800 Series Matrix Switchers do not support a multi-screen view as a stand alone system. This will require the installation of a GENEX Multiplexer as a secondary system to be interfaced with CM6700/CM6800 Series Matrix Switcher. Once all programming and physical connections are made, the multi-screen buttons on the KBD300A, KBD200A and KBD960 will function accordingly. Both the Simplex and Duplex Series multiplexers are compatible with the CM6700/CM6800 Series Matrix.

  • View LL#11516 for operation of KBD300A to Genex with Matrix.