Are the GV NC201B and GV NC201VA compatible with DS?

Issue

Are the GV NC201B and GV NC201VA compatible with DS?

Product Line

Pelco Video Management

Environment

  • Digital Sentry
  • GVI GV-NC201B camera
  • GVI GV-NC201VA camera

Cause

Check compatibility between the two equipment if it's possible to have the Digital Sentry recorder to record IP camera model GV-NC201B and GV-NC201VA.

Resolution

No. Currently, they are not supported by Digital Sentry systems. For all supported IP camera, see article Digital Sentry IP Camera Compatibility: What Pelco/Third-Party IP cameras are supported on the Digital Sentry (DS) System?