What software is needed when connecting to a DX8100 Series hybrid video recorder on the network?

Issue

What software is needed when connecting to a DX8100 Series hybrid video recorder on the network?

Product Line

Pelco Video Management

Environment

  • DX8100 Series HVR
  • Remote Client

Cause

Client applications for DX8100 Series HVR

Resolution

Either of the following client software can be used:

  • The DX8100 Client (PC Client software).
  • DX Series Client.
  • DX8100 Series Web Client using Internet Explorer v6.0 and v7.0. Refer to the specification sheet for up-to-date version support.
  • DS ControlPoint version 1.5 or later

Download the DX8100 Client and DX Series Client

 

Download DS ControlPoint:

  1. Refer to article "Where can I download the latest version of DS ControlPoint client software?" for instructions and location to download the DS ControlPoint.