Can the NET5402R-HD display video from the NET5301T?

Issue

Can the NET5402R-HD display video from the NET5301T?

Product Line

Pelco Video Management, Pelco Transmission & Power

Environment

  • Endura NET5402R-HD- All versions
  • Endura NET5301T- All versions

Cause

New HD decoder is purchased but need to know if the video from the older encoders can be viewed on it.

Resolution

Yes. The NET5402R-HD is capable of displaying video from a NET5301T. Please note that these devices will not function in a stand-alone operation and they require a complete Endura system in order to communicate.