How do I change the Snapshot configuration settings on the Endura WS5070?

Issue

How do I change the Snapshot configuration settings on the Endura WS5070?

Product Line

Pelco Video Management

Environment

Endura WS5070- All versions

Cause

It is desired that the snapshot settings be modified

Resolution

  1. Access the Setup screen:
    • Click the Setup button in the toolbar.
    • Use the keyboard shortcut (CTRL + Shift + S)
  2. Click on the Users tab.
  3. Choose the desired user.
  4. Set up the default directory for snapshot files. Type the path in the Default Directory box. Or click “...” to browse through a list of available directories that you want to use.
  5. Select the default snapshot format from the drop-down list:
    • Portable Network Graphics files (*.png, default)
    • Bitmap Files (*.bmp)
    • JPEG files (*.jpeg, *.jpg)
  6. Click Apply to save the settings.
  7. Click OK to exit and save the settings (if not already saved through Apply) or click Cancel to exit without saving the new settings.