How do I change the Export configuration settings on the Endura WS5070?

Issue

How do I change the Export configuration settings on the Endura WS5070?

Product Line

Pelco Video Management

Environment

Endura WS5070- All versions

Cause

It is desired that the export settings be modified.

Resolution

Follow the following steps to change the Export configuration settings.

  1. Access the Setup screen:
    • Click the Setup button in the toolbar.
    • Use the keyboard shortcut (CTRL + Shift + S
  2. Click on the Users tab.
  3. Choose the desired user.
  4. Set the default directory for exported files. Type the path in the Default Directory box. Or click “...” to browse through a list of available directories that you want to use.
  5. Select the default export format from the drop-down list:
    • Pelco Video Files (*.pef, default). This format works only on the Pelco Endura Player. It allows you to view overlays and authenticate exported video and audio files.
    • Apple QuickTime MPEG-4 files (*.3gp). This format works on most media players; however, in QuickTime format, video cannot be authenticated.
  6. Click Apply to save the settings.
  7. Click OK to exit and save the settings (if not already saved through Apply) or click Cancel to exit without saving the new settings.