Is it okay to have a UDI5000-CAM total capacity utilization at 100%?

Issue

Is it okay to have a UDI5000-CAM total capacity utilization at 100%?

Product Line

Pelco Video Management

Environment

Endura UDI5000-MTRX- All versions

Cause

Information regarding capacity utilization for the UDI5000-MTRX is needed.

Resolution

No. If the total capacity utilization is at or above 100% when adding 3rd party cameras, this can cause video streams to become unstable. Therefore, the camera will drop offline and/or not get recorded.