What mounting options are available for the SM5000?

Issue

What mounting options are available for the SM5000?

Product Line

Pelco Video Management

Environment

Endura SM5000- All versions

Cause

Information on mounting options for the SM5000 is needed.

Resolution

The SM5000 can be mounted on a desktop or into an industry-standard 19-inch equipment rack. All accessories are included with the unit.