How can I configure the Endura VCD5200 Series video console display unit locally?

Issue

How can I configure the Endura VCD5200 Series video console display unit locally?

Product Line

Pelco Video Management

Environment

Endura VCD5200- All versions

Cause

Information regarding the configurations that are available locally on a VCD5200 is needed.

Resolution

You can configure the VCD5200 Series using an Endura keyboard KBD5000 or with a PC keyboard and mouse.

Please note that the following options are available on the VCD5200 Series. All other Endura configuration must be done via the Endura WS5000 Advanced Management Software.

VCD5200 Configuration Options: