How to switch between VGA and analog BNC monitors on the DX Series DVRs and HVRs recorder.

Issue

How to switch between VGA and analog BNC monitors on the DX Series DVRs and HVRs recorder.

Switch monitor

Product Line

Pelco Video Management

Environment

  • DX4500/DX4600
  • DX4700/DX4800(HD)

Cause

DVR/HVR system information not displaying on the connected VGA or analog BNC display.

Change view between VGA to BNC or vise versa.

Resolution

DX4500/DX4600

Switch Monitor

  • VGA Output: On the front panel press and hold the MAIN button. After approximately five seconds the system will beep and restart. Verify the main video display on the VGA monitor.
  • BNC MAIN Output: On the front panel press and hold the SPOT button. After approximately five seconds the system will beep and restart. Verify the main video display on the analog monitor.



DX4700/DX4800DX4700/DX4800 (HD) 

  • The DX4700/DX4800 standard series and DX4700/DX4800 (HD) series do not require manual switching between video outputs, the VGA and BNC Main outputs are both active.

     

DX4500/DX4600 Rear Panel: