Will the DX4500/DX4600 DVR support coaxitron protocol?

NOTICE

DISCONTINUED PELCO PRODUCT.
This product has been discontinued. For further information please visit pelco.com/support/discontinued-products

Issue

Will the DX4500/DX4600 DVR support coaxitron protocol?

Product Line

Pelco Video Management

Environment

  • DX4500 v1.3
  • DX4600 v1.3

Cause

Early version of DX4500 and DX4600 series hardware does not support coaxitron protocol.

Resolution

The DX4500 or DX4600 model that supports coaxitron is DX4500C or DX4600C respectively.

Follow the steps below to confirm if the recorder support coaxitron.

  1. Log in to the DX4500/DX4600 recorder.
  2. Click on the system information button on the tool bar. The System Information page appears.
  3. Check if the model name is DX4500C/DX4600C.
  4. Check if the version is 1.3 or higher
    If the recorder is DX4500C/DX4600C and running on 1.3 or higher, the recorder support coaxitron.

NOTE: If the model name is DX4500/DX4600, the recorder requires RS-485/RS-422 or CM9760-CXTA Coaxitron Translator for PTZ.