Backup the CM9700-CC1 flat files.

Issue

How can I backup the CM9700-CC1 flat files?

Product Line

Pelco Matrix

Environment

CM9700-CC1

Cause

For recovery use.

Resolution

Copy the files to a spare floppy disk by completing the following steps:

  1. From your system keyboard, select CONTROL Q to bring the system to DOS prompt.
  2. At the C:\9700> prompt, type the command copy filename.* a:
    NOTE: If your flat files were named node1, then the command would look like this copy node1.* a:
  3. Press Enter key