What is the maximum number of controllers (users) for the CM6700 and CM6800 Matrix Switchers?

Issue

What is the maximum number of controllers (users) for the CM6700 and CM6800 Matrix Switchers?

Product Line

Pelco Matrix

Environment

  • CM6700 Matrix switcher all versions
  • CM6800 Matrix switcher all versions

Cause

Documentation is currently not available

Resolution

The CM6700 provides switching and control for 16 video inputs and up to 4 monitor outputs from any one of up to 8 keyboards.
The CM6800 provides switching and control from any one of up to 10 keyboards. The system can also be used to control other devices, such as Genex® multiplexers.