What are the programming parameter settings for the CM9700 Series Matrix Switcher Sercom ports?

Issue

Not clear on which ports are intended for certain peripheral devices.

Product Line

Pelco Matrix

Environment

  • CM9760-CC1 all versions
  • CM9700-CC1 all versions

Cause

Peripheral devices are not coming online.

Resolution

The baud rate and parity settings for the CM9700 Series Matrix Switcher are user definable, and set per device.