Power Supply and Power Cord for the CM9760-KBD Intelligent Keyboard.

Issue

CM9760-KBD Intelligent Keyboard will not power up.

Product Line

Pelco Matrix

Environment

CM9760-KBD Intelligent Keyboard all versions

Cause

Power supply and power cord is required for replacement.

Resolution

Yes. The matrix itself does not supply power to the CM9760-KBD. The following parts must be ordered to power the keyboard:

  • PS01-3002-9015G power supply and select the proper country power cord P/N below:

Note: The CM9760-KBD keyboard when originally ordered from factory, is provided with a power supply and power cord.