What is the maximum number of camera inputs per node for the CM9780 Matrix Switcher/Controller?

Issue

What is the maximum number of camera inputs per node for the CM9780 Matrix Switcher/Controller?

Product Line

Pelco Matrix

Environment

CM9780 Matrix Switcher all versions

Cause

Specifying a Matrix Switcher

Resolution

The maximum number of camera inputs per node is 4,096 cameras.