Will the Spectra Mini camera support Power over Ethernet (PoE)?

Issue

Will the Spectra Mini camera support Power over Ethernet (PoE)?

Product Line

Pelco Cameras, Pelco Transmission & Power

Environment

Spectra Mini

Cause

Power the Spectra Mini Dome system over ethernet cable is not supported. The Spectra Mini is prewired for 24 VAC.

Resolution

No, the Spectra Mini requires input voltage of 18 to 30 VAC; 24 VAC nominal and input power of 21 VA nominal.

The Spectra Mini IP Network Dome System is IEEE 802.3af PoE compatible, which supplies power to the unit through the network.