After the Spectra IV Series TXB-IP or TXB-N is installed, can I control PTZ control over a network?

Issue

After the Spectra IV Series TXB-IP or TXB-N is installed, can I control PTZ control over a network?

Product Line

Pelco Cameras

Environment

  • Spectra IV Series
  • TXB-IP
  • TXB-N
     

Cause

The TXB-IP or TXB-N translator boards is a network-based communication module that add IP connectivity to the Spectra IV camera system.

Resolution

Yes. The TXB-IP and the TXB-N are modules that go into the Spectra IV to allow video and control over a network.