What is the maximum number of P protocol addresses the CM9700 Matrix will support per sercom port?

Issue

What is the maximum number of P protocol addresses the CM9700 Matrix will support per sercom port?

Product Line

Pelco Matrix

Environment

CM9700-CC1 any version

Cause

Installing multiple PTZ cameras.

Resolution

The recommended number of P addresses is 32 per port, with the addition of multiple CM9760-CDU-T (code distribution unit) up to 254 is possible.