Installing the NEMA back box to IP110/IP111 series cameras wiring issue.

Issue

Installing the NEMA back box to IP110/IP111 series cameras wiring issue.

Product Line

Pelco Cameras

Environment

  • NEMA back box
  • IP110/IP111 Series

Cause

The NEMA back box can pinch the loose wires from the IP110 camera.

Resolution

When installing the NEMA back box to IP110 series cameras, care must be taken to keep the wiring together with a wire tie or electrical tape. When the wires are loose, the back box can pinch the wires which can cause problems. Although production will begin using a wiring tie to bundle the wires to prevent the pinching, there may be units in the field that can eventually fail due to this issue.

The attached photos illustrate the pinched wires.





Source: TT090721IE