Upgrades to the Spectra Mini to address issues regarding losing focus, video and preset locations.

Issue

Upgrades to the Spectra Mini to address issues regarding losing focus, video and preset locations.

Product Line

Pelco Cameras

Environment

  • SD4-W0
  • SD4-B0

Cause

Loss of Focus occurs for Spectra Mini.

Resolution

Over the last six months, there have been upgrades to the Spectra Mini to address issues regarding the Spectra Mini losing focus, video and preset locations.

The upgrades are listed below:

LOSING FOCUS AND VIDEO
 
Venting fins have been added to the dome liner, this helps keep the camera cooler. The new part number is:
 
Dome Liner: MF00-4650-009C
 
To keep the camera cooler, the motor bracket, heat conductive pads and camera cover have all been changed to a thicker measurement which allows better heat transfer. The new part numbers are:
 
Motor Bracket: MF00-4650-008C
 
Heat Conductive Pads: MF00-6110-015A
 
Camera Cover: MF11-4650-050C
 
The pan bearing assembly and the tilt bearing assembly have been changed to allow for the new size of the motor bracket. The new part numbers are:
 
Pan Bearing Assembly: Mf00-4651-012B
 
Tilt Bearing Assembly: MF00-4651-001B

LOSING PRESET LOCATION 

The slip ring has been changed to allow the optical sensor to see the flag arm better. The flag arm is now held to tighter specifications allowing it to pass through the optical sensor at an optimum position. This change allows for the proper home position when the camera is configured. The new part number is:

Slip Ring: MF00-4651-030C

Source: TT090504SP