Tungsten Palm One - Changing the Baud Rate

Issue

How to adjust the baud rate on the Tungsten Palm One.

Product Line

Pelco Cameras

Environment

  • IPS-RMK
  • Tungsten Palm One

Cause

Palm One to PC baud rate matching

Resolution

  1. From the home screen, click on the Prefs Icon
  2. Click Connection
  3. Click on the connection that you are going to use
  4. Click Edit
  5. Click Details
  6. From the Speed details, select the down arrow
  7. Choose Baud Rate
  8. Click OK (The baud rate will now be set to the newly selected rate.)