Should the Endura UDI5000-CAM universal device interface appear in the EnduraXpress EE5000 web configuration page?

Issue

Should the Endura UDI5000-CAM universal device interface appear in the EnduraXpress EE5000 web configuration page?

Product Line

Pelco Video Management

Environment

  • Endura EE500- All versions
  • Endura UDI5000-CAM- All versions

Cause

Information regarding the appearance of the UDI5000-CAM from the web interface of the EE500 is needed.

Resolution

No. The UDI5000-CAM is designed to allow third-party IP cameras to easily and transparently interface to the Endura® system. Only cameras will appear in the web configuration page.